Technical FAQs

Ask a Question

What is the torque requirement for the WBS on an aluminum lug for the L frame Powerpact breaker?

The torque for all aluminum lugs (AL400L61K3, AL600LS52K3, AL600LF52K3) is 50 N-m or 442 lb.-in.

CTA-ID : 2060046
Was this helpful?
What can we do to improve the information ?