Technical FAQs

Ask a Question

What is the wire range for the lugs provided on the EZM11600GCBC EZM Main Circuit Breaker?

Issue:
Wiring

Product Line:
EZM

Cause:
Terminal lug range

Resolution:
The factory installed line side lugs will accept (6) #1/0 AWG - 750 KCMIL or (12) #1/0 AWG - 250 KCMIL copper or aluminum conductors per phase and neutral. See the CAD drawing #PWFDS-SYRS-0005 for alternate lugs. Link provided below.

http://static.schneider-electric.us/docs/Electrical%20Distribution/Metering%20Equipment/EZ%20Meter-Pak-Multi%20Metering/EZM/PWFDS-SYRS-0005.pdf


CTA-ID : 2060006
Was this helpful?
What can we do to improve the information ?