Technical FAQs

Ask a Question

Why is there a gap in the bussing in a EZM1800FS, between the MHP26000 switch and thru bus?

The gap is where 300VAC Class T fuses are to be installed.


CTA-ID : 2060026
Was this helpful?
What can we do to improve the information ?