Technical FAQs

Ask a Question

What are the repair parts for a HOM2040M200RB, Series S01 load center?

Issue:
older design repair parts

Prouduct line:
Homeline load centers

Environment:
repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable.
Cover - 4054802204
Cover Mounting Screw - 2142717161 (2 Required)
Interior Trim - 4056503801 (TRIM FOR SERIES S01 is Obsolete and No Longer Available, with NO replacement)
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - HOM2040M200RBI (Obsolete, NLA order HOM2040M200PRBI)
Main Breaker - QOM2200VH
Neutral Bonding Screw - 4028345850K
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2059971
Was this helpful?
What can we do to improve the information ?