Technical FAQs

Ask a Question

Is the XVC product line suitable for outdoor use?

Yes, this is IP54 (NEMA 12 & 3R) rated.

*Per 9001HO0905 document.



CTA-ID : 2059760
Was this helpful?
What can we do to improve the information ?