Technical FAQs

Ask a Question

What is a 9080V3?

The 9080V1, V2 and V3 are now obsolete. Possible replacements would be the 9080G terminal block line, selection based on customer application.
The 9080V1, V2 & V3 are a hard phenolic panel mount terminal block with solder-less box lugs. The conductor range is #6 to 250 kcmil. The 9080V1 has 1 circuit, V2 has 2 and V3 has 3 circuits. They are shown in digest 170 page 20-19.
Was this helpful?
What can we do to improve the information ?