Technical FAQs

Ask a Question

What is the replacement for a 9001TB contact block?<br>

This was 2 NO and 2 NC contacts. The 9001TAD1 adapter that allowed using the 9001KA1 contacts is obsolete. Entire operator will need to be crossed to the 9001K line of pushbuttons.

CTA-ID : 2059953
Was this helpful?
What can we do to improve the information ?