Technical FAQs

Ask a Question

What is the NEMA rating or IP degree of protection for the door-mounted 32598 RE12 and 32600 RE22 rotary handle operator for the Powerpact D frame (and NSJ) breaker?

32598 and 32600 are IEC-Style Door-Mounted Rotary Operating Handles.  The handle mechanism can be used in NEMA 3R and 12 enclosure applications.  Degree of protection: IP40 per IEC 529.

CTA-ID : 2059919
Was this helpful?
What can we do to improve the information ?