Technical FAQs

Ask a Question

What is the replacement for the 29340 handle mechanism kit?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The catalog number has been changed to globally align the numbering system.
The 29338 is the standard black handle replaced with the part number  S29338, the 29340 is the red handle on yellow bezel the part number is S29340. The telescopic handle for drawout mounting is number 29343 and it is now a S29343.


CTA-ID : 2059939
Was this helpful?
What can we do to improve the information ?