Technical FAQs

Ask a Question

When a programmed authorization card is used to activate a dual charger with RFID access, catalog number EV230PDRR, are both sides of the charger activated, or just one side?

Issue:
Product Design Feature

Product Line:
EVSE

Cause:
Clarification of the design and features

Resolution:
Both sides are activated for a period of 2 minutes. A vehicle must be connected (either side) within 2 minutes to activate charging. If a vehicle is connected to one side of the charger, the other side will de-energize and not be useable after 2 minutes of the authorization car being scanned.
Was this helpful?
What can we do to improve the information ?