Technical FAQs

Ask a Question

What is the UTS3 test kit error message ``current driver overvoltage``?

While using the Series B test module: This is a normal error when not connected to the breaker.
While using the Self Test module: This could mean a bad transistor in the test kit. Will probably see smoke coming from test kit.


CTA-ID : 2059892
Was this helpful?
What can we do to improve the information ?