Technical FAQs

Ask a Question

Can you remotely read values such as Average instantaneous current in A phase as indicated in Micrologic H manual 48049-330-03 page 86. The register list does not show a register for this; closest is Current Apparent A on page 105.

Unfortunately, the Average Instantaneous Current per Phase is not a value calculated by the trip unit and therefore is not available over Modbus. The only average current is between all phases and is located in register 1027. If they would like the current going through a phase at any one time, they should be reading the demand current on registers 2200, 2201, 2202, and 2203 for Phase A, Phase B, Phase C, and Neutral, respectively. In this case it seems that our documentation is misleading.


CTA-ID : 2059816
Was this helpful?
What can we do to improve the information ?