Technical FAQs

Ask a Question

What is the difference between a DECAP and a DPCAP?

REVISON TO FAQ 12531: THE DECAP AND DPCAP DEVICES ARE NOW OBSOLETE WITH NO REPLACEMENT.

The DECAP is the closing cap for the E type inserts, and the DPCAP is the closing cap for the P type inserts on the subway system.


CTA-ID : 2059707
Was this helpful?
What can we do to improve the information ?