Technical FAQs

Ask a Question

Please confirm that the Neutral can be connected to either the left hand or the right hand pole in a Masterpact 4-pole breaker.

The 4 neutral pole is specific. So a circuit breaker either comes equipped with a neutral pole configured on the far right pole or the far left pole. The pole is marked and must be wired accordingly because the trip system for the neutral set up separate form the 3 phases.


CTA-ID : 2059750
Was this helpful?
What can we do to improve the information ?