Technical FAQs

Ask a Question

REVISION TO RESOLUTION 2025325: correct wording from `of 100A busway` to `or 100A Powerbus` Can I get a replacement for a catalog number AP14, which is a 10 foot piece of 100A busway?

The AP14 busway is obsolete and unavailable.  However, you can use a PTB14 tap box (and a ground kit PGKFA2, if using an AP14G type busway)  and cable over to a new run of 100 amp rated Powerbus225.
Was this helpful?
What can we do to improve the information ?