Technical FAQs

Ask a Question

What is the degree of protection of the XB5 Harmoney 22 MM Biometric switches?

They are rated for IP65, NEMA 1, 2, 3, 3R and 12.


CTA-ID : 2059706
Was this helpful?
What can we do to improve the information ?