Technical FAQs

Ask a Question

Are the Zelio RSL Relays Din Rail Mountable?

Yes, it is din rail mountable on 1.38 in. (35 mm) DIN rail.


CTA-ID : 2059732
Was this helpful?
What can we do to improve the information ?