Technical FAQs

Ask a Question

Is the 9007MS10G0300 available with a 33 foot cord?

Yes change the part number from the 9007MS10G0300 to a 9007MS10G1300 to get it with a 33 foot cord. Remember not all part numbers can be constructed from the forms available in the Digest, so verify the part number in Quote to Cash after identifying it and before placing an order

CTA-ID : 2059517
Was this helpful?
What can we do to improve the information ?