Technical FAQs

Ask a Question

Does Square D offer an alternate main breaker to replace the 100A in a QO112M100 load center?

Issue:
Product Feature

Product Line:
QO Load Center

Cause:
Alternate main breaker

Resolution:
The factory installed 100A main breaker is a QOM1-VH frame size, Catalog Number QOM100VH. The alternate QOM1-VH Main Breaker Kits that could replace the QOM100VH would be:
50A = QOM50VH
60A = QOM60VH
70A = QOM70VH
80A = QOM80VH
90A = QOM90VH
100A = QOM100VH

A maximum 100A breaker can be used. 



CTA-ID : 2059656
Was this helpful?
What can we do to improve the information ?