Technical FAQs

Ask a Question

Can the QO612L100 and/or QO816L100 Load Centers be converted to a main breaker panel by adding a QOM-VH Main Breaker Kit?

Issue:
Application

Product Line:
QO Load Center

Cause:
Application

Resolution:
These load centers are considered "fixed" main lugs load centers and will not accept the QOM-VH Main Breaker Kits. If a main breaker is required, consider backfeeding a 2 Pole branch breaker on the interior. A PK2MB Retaining Kit would be also be required to retain the backfed breaker onto the interior.


CTA-ID : 2059546
Was this helpful?
What can we do to improve the information ?