Technical FAQs

Ask a Question

Does the J250R circuit breaker enclosure have enough wire bending space to allow for the use of compression lugs on the H & J Frame circuit breakers?

The compression lugs were not evaluated in these enclosures with UL. The plant would need to physically check to determine if there is enough wire bending space for both the H & J Frame breakers.

CTA-ID : 2059645
Was this helpful?
What can we do to improve the information ?