Technical FAQs

Ask a Question

What is the torque requirement for lugs for the Powerpact L frame breaker?

The torque requirement for the following lugs is 50 N-m or 442 lb.-in.
AL400L61K3, AL600LS52K3, CU600LS52K3, AL600LF52K3, CU600LF52K3

The torque requirement for lug CU400L61K3 is 31 N-m or 275 lb.-in.
 

CTA-ID : 2059561
Was this helpful?
What can we do to improve the information ?