Technical FAQs

Ask a Question

What wire sizes does the PDC5DG20 accept?

The correct wire range is (3) 14 - 1 AWG and (2) 3 - 2/0 AWG. The D frame catalog is incorrect. The L frame breaker uses the same lug (different catalog number, PDC5DG20L3); L frame catalog and Digest 176 has correct information for PDC5DG20L3 (which is the same as PDC5DG20).

CTA-ID : 2059568
Was this helpful?
What can we do to improve the information ?