Technical FAQs

Ask a Question

The XALD341 replacement is a XALD351H29H7: is there significant change from the old part number to the new part number?

Issue:
The XALD341 replacement is a XALD351H29H7: is there significant change from the old part number to the new part number?

Product Line:
22mm Control Stations  

Environment:
XALD 22mm Control Stations.     

Cause:
Clarify the difference between the 2 different part numbers.                                                       

Resolution:                                                                 
H29 means the legend plate has english verbiage. H7 means it is UL and offers English instructions. It will also have a 1/2 inch conduit entry and a ground screw.
In an effort to align globally with the pendant catalog numbering system, it was necessary to add the suffix H7and H29 to some XAL catalog numbers.
The insignificant changes in the XAL Control Station product has no particular functional impact.
Was this helpful?
What can we do to improve the information ?