Technical FAQs

Ask a Question

How do you program alarms into the Micrologic 5 and 6 series trip units for Powerpact H, J, and L frame breakers?

Alarms cannot be set using the keypad or the front display module. They are set through the communication network with the PC. Set-up includes the threshold, priority, activation delay before display and deactivation delay. It is also possible to reprogram the standard assignment for the two SDx relay outputs to user-selected alarms.

CTA-ID : 2059352
Was this helpful?
What can we do to improve the information ?