Technical FAQs

Ask a Question

Is the ZB5AP plastic 22mm clear booted pushbuttons being replaced with the ZB5APA?

Yes. The following crosses are to align globally our current catalog or part idenfication numbering sytstem:
ZB5AP1 ZB5APA1 NON-ILLUM CLEAR BOOT - WHITE FLUSH
ZB5AP2 ZB5APA2 NON-ILLUM CLEAR BOOT - BLACK FLUSH
ZB5AP3 ZB5APA3 NON-ILLUM CLEAR BOOT - GREEN FLUSH
ZB5AP4 ZB5APA4 NON-ILLUM CLEAR BOOT - RED FLUSH
ZB5AP5 ZB5APA5 NON-ILLUM CLEAR BOOT - YELLOW FLUSH
ZB5AP6 ZB5APA6 NON-ILLUM CLEAR BOOT - BLUE FLUSH




CTA-ID : 2059346
Was this helpful?
What can we do to improve the information ?