Technical FAQs

Ask a Question

Is the 9421NTS30 terminal shield for both the line and load terminals?

Yes, it is for use with the Line or Load terminals on a 30A Disconnect Switch .


CTA-ID : 2055095
Was this helpful?
What can we do to improve the information ?