Technical FAQs

Ask a Question

What is the largest amperage of back fed main breaker that can be used in a QO148L125GS load center?

The largest back fed main breaker that can be used would be a 125A double pole. A PK2MB Retaining Kit would also be required to secure the back fed main breaker to the load center interior.


CTA-ID : 2055418
Was this helpful?
What can we do to improve the information ?