Technical FAQs

Ask a Question

What is the largest amperage of branch breaker that can be used in a QO148L125GS load center?

The largest branch breaker that can be used would be a 70A single pole or a 125A double pole.


CTA-ID : 2055415
Was this helpful?
What can we do to improve the information ?