Technical FAQs

Ask a Question

What is a SMS224M?

Issue:
What is a SMS224M?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
THIS DEVICE WAS NEVER MANUFACTURED. HOWEVER, THE FOLLOWING INFORMATION WOULD BE APPLICABLE TO OTHER SMS MAIN SWITCH DEVICES THAT WERE MANUFACTURED AND IS BEING PROVIDED TO ASSIST YOU IN UNDERSTANDING SOME BASIC INFORMATION CONCERNING THE SMS PRODUCT LINE:
This device is a panel mounted fusible main switch. It is similar to the QMB switch product line, except it was designed to bolt onto the panel bus bars with a strap (SMS = Strap Mounted Switch), rather than plugging on. It was designed in cooperation with, and only sold to, Mac Products (an OEM in New Jersey). The switch was used in a panel of Mac Products design and manufacture. The switch was produced for Mac Products in the 2004-2005 time frame. Mac Products exited the panel building business shortly thereafter. They are no longer supporting the SMS panel board. The SMS switch is now obsolete and no longer available. Due to the mounting differences, a QMB switch could not be substituted for a SMS switch.


CTA-ID : 2055399
Was this helpful?
What can we do to improve the information ?