Technical FAQs

Ask a Question

What are the repair parts for the H362AWH, series F6 (may be shown as F06)?

Current Design Repair parts

Product Line:
Heavy Duty Safety Switches

Repair parts



.The repair parts for the H362AWH, series F6 (F06) are as follows. No other parts are available.

-Line Base Assembly -4056603850 (requires one per switch. Arc suppressor assembly not included)
-Load Base Assembly - 4056604050 (requires one per switch)
-Line and Load Base Mounting Screw - 4020515101(3 for line & 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one per switch)
-Arc Suppressor Mounting Screw - 4020514501
-Handle/Mechanism kit - HMR06FN12WH (includes handle, mechanism, rod, and lockplate)
-Line/Load lugs - 4025101652 (3 each for line and load base assembly)
-Line/Load Lug mounting screw - 4020514202 (one required per lug)
-Receptacle - 4051117350
-Receptacle Mounting Screws - 2142717161 (required 4)

CTA-ID : 2055408
Was this helpful?
What can we do to improve the information ?