Technical FAQs

Ask a Question

Can we provide factory installed legend plates on Heavy Duty safety switches?

Yes, refer to the Supplemental and Obsolescence Digest 175, page 2-3. They cannot be provided on NEMA 7/9 devices.


CTA-ID : 2055400
Was this helpful?
What can we do to improve the information ?