Technical FAQs

Ask a Question

Are the `Close and Latch` ratings for the NW are symmetrical or assymetrical? In other words, RMS or peak with offset?

The ``close and latch`` ratings are RMS values based on an asymmetrical first half cycle.

CTA-ID : 2055066
Was this helpful?
What can we do to improve the information ?