Technical FAQs

Ask a Question

Is the VW3A1105 RJ-45 adaptor required when remote mounting the ATV61/71 keypad?

The adaptor component is required to interface between the cable and the LCD keypad if you do not have the remote mounting bezel VW3A1102. If you use the remote mounting kit VW3A1102 this RJ45 is part of the bezel and will not be needed.


CTA-ID : 2055068
Was this helpful?
What can we do to improve the information ?