Technical FAQs

Ask a Question

Is there a lug kit for the Powerpact PG circuit breakers for use with (2) 600 kcmil cables?

Use AL800P6K for (2) 600 kcmil conductors per phase for the Powerpact P frame breaker.
Note that it does not fit onto ON end of unit-mount P-frame circuit breakers.


CTA-ID : 2031228
Was this helpful?
What can we do to improve the information ?