Technical FAQs

Ask a Question

Is the H100XFA-1212 suitable for use as service equipment?

Yes, this enclosed molded case switch is labeled as ``Suitable for use as Service Equipment``. If used on a 3 Phase/4 Wire system, a neutral should be purchased separately and field installed. For service equipment use, the neutral (once it is installed) should be bonded to the enclosure with the bonding means provided with the neutral assembly. Use 100SNA neutral assembly, if required.


CTA-ID : 2055222
Was this helpful?
What can we do to improve the information ?