Technical FAQs

Ask a Question

30A LK3DU3, 60A LK3GU3, and 100A LK3JU3 unfused switches - why are terminal shrouds not offered?

Per GIC Help File: Additional shielding is not required because the lugs are recessed into the switch body which provides the required shielding.

CTA-ID : 2054989
Was this helpful?
What can we do to improve the information ?