Technical FAQs

Ask a Question

What are the repair parts for a HU366R Series E2 and E4 Heavy Duty Safety Switch?<br /><br />

The parts listed here are the only field replaceable parts.
Complete interior - HUN366E2 (includes line base assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-186-50 SEL (3-required and arc suppressor assembly is not included)
Arc suppressor assembly - 40512-708-50 SEL (3-required) Obsolete and replaced by 40512-708-50 (3-required)
Lug assembly - 44050-446-01 (2 required per base assembly)
Line base phase insulator - 40552-193-01 (2 required)
Line base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Door thumb retainer - 44050-490-01
Door thumb screw - 44050-434-01
Handle knob kit (black & red knob at end of handle) - Series E2 is 44011-427-50, Series E4 is 40283-435-50


CTA-ID : 2054908
Was this helpful?
What can we do to improve the information ?