Technical FAQs

Ask a Question

Are the HU361SS, HU362SS, HU363SS, HU364SS, HU365SS and HU366SS safety switches suitable for use as service equipment?

Issue:
Application

Product Line:
HD Safety Switch

Cause:
Application

Resolution:
Yes, these switches are marked: "Suitable for use as service equipment``. If used on a 3 Phase/4 Wire system, a neutral should be purchased separately and field installed. For service equipment use, the neutral (once it is installed) should be bonded to the enclosure with the bonding means provided with the neutral assembly.


CTA-ID : 2055192
Was this helpful?
What can we do to improve the information ?