Technical FAQs

Ask a Question

Can the coils of a Ventilated Transformer be replaced? I know a Sealed Resin Epoxy Encapsulated Transformer cannot have its coils replaced.

Issue:
Coil replacement

Product Line:
LV Transformers

Environment:
Applies to Ventilated and Non-Ventilated Transformers by SquareD/Schneider Electric

Cause:
Coil failure on a Transformer

Resolution:

Yes, but it is generally not practical from a cost or lead time standpoint to replace coils in Transformers. New coils must be wound. The damaged coil(s) cannot be removed without unstacking the steel laminated core, which is a time-consuming, meticulous process. Only factory personnel, trained and authorized to repair Transformers are allowed attempt to replace the coils.


CTA-ID : 2055104
Was this helpful?
What can we do to improve the information ?