Technical FAQs

Ask a Question

Is the HU362DX safety switch suitable for use as service equipment?

Yes, this switch is labeled as ``Suitable for use as Service Equipment``. If used on a 3 Phase/4 Wire system, a neutral should be purchased separately and field installed. For service equipment use, the neutral (once it is installed) should be bonded to the enclosure with the bonding means provided with the neutral assembly. Use H60SN neutral assembly, if required.


CTA-ID : 2055210
Was this helpful?
What can we do to improve the information ?