Technical FAQs

Ask a Question

<br /><br />Can an I-Line panelboard having a main breaker greater than 800A be supplied with a 200% neutral?

Issue:
Can an I-Line panelboard having a main breaker greater than 800A be supplied with a 200% neutral?

Product Line:
I line panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
An I-Line panelboard with a main breaker greater than 800A cannot be supplied with a 200% neutral.


CTA-ID : 2054994

Was this helpful?
What can we do to improve the information ?