Technical FAQs

Ask a Question

Can I order a 200% neutral for an enclosed circuit breaker?

Yes, but only for the FA , KA, and LA breakers. The FA frame breaker can be installed in a KA enclosure NEMA 1 or 3R enclosure and used with the SN225KA neutral to accommodate up to 225A. The KA frame breaker can be installed in an LA enclosure NEMA 1 or 3R enclosure and used with the 400SN neutral to accommodate up to 400A. The LA frame breaker can be installed in an MA enclosure NEMA 1 or 3R enclosure and used with the SN1000ma neutral to accommodate up to 1000A.
NOTE: Check quantity and size of lug terminations available on the neutral assembly prior to pulling neutral conductor(s) to insure availability of termination points.
ALSO NOTE: KA and MA breakers are now obsolete and the MA frame enclosures are also obsolete.



CTA-ID : 2054913
Was this helpful?
What can we do to improve the information ?