Technical FAQs

Ask a Question

The 8910 definite purpose contactors - will `old` style auxiliary contacts mount to `new` style contactors and vice versa? Are series B<br />accessories compatible with series C devices

Issue:
The 8910 definite purpose contactors - will `old` style auxiliary contacts mount to `new` style contactors and vice versa? Are series B
accessories compatible with series C devices

Product Line:
Definite Purpose Contactors

Environment:
Products sold and used in the United States

Cause:
Using old auxiliary contacts on new contactors

Resolution:
No. Obsolete Series B 8910 contactors will accept only Series B auxiliary contacts (9999D**) while current Series C 8910 contactors will accept only Series C auxiliary contacts (9999DD**).


CTA-ID : 2055183
Was this helpful?
What can we do to improve the information ?