Technical FAQs

Ask a Question

What information must be supplied on the label to indicate UL listing of a circuit breaker?

The minimum UL requirements for marking are:
The UL listing mark.
The words listed circuit breaker or listed c. b.
An issue number

The UL and CSA listing marks are there to show that the product was UL/CSA certified at the time of manufacture.

Our UL/CSA equipment should also be marked with similar information.


CTA-ID : 2055067
Was this helpful?
What can we do to improve the information ?