Technical FAQs

Ask a Question

9001TF: Is there anything that will replace this?

Will need to replace with two 9001KA1`s and one 9001TAD1 liner kit.
The 9001TAD1 is now obsolete. Without it the 9001KA contacts cannot be mounted on the Type T operators.



CTA-ID : 2054952
Was this helpful?
What can we do to improve the information ?