Technical FAQs

Ask a Question

What are the repair parts for a H465AWK Series E2 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Complete interior - HN465AE2 (includes line & load base assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-210-50 SEL (4-required and arc suppressor assembly is not included)
Load base assembly - 40552-211-50 SEL (4-required)
Arc suppressor assembly - 40512-708-50 SEL (4-required) (OBSOLETE replaced by 4051270850)
Small lug assembly - 40560-270-50 (COPPER LUG/OBSOLETE)
Small lug Replacement- 40251-136-50 (Aluminum Lug Replacement/will accept Al/Cu Conductors)
Large lug assembly - 40256-026-50 (requires one per base assembly)
Line base phase insulator - 40512-014-01 (3 required)
Load base phase insulator - 40552-191-01 (3 required)
Line & load base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Vault handle - 40512-194-50 SEL
Handle knob kit - 40283-435-50 (the black & red knob at the end of the handle)


CTA-ID : 2054942
Was this helpful?
What can we do to improve the information ?