Technical FAQs

Ask a Question

What are the repair parts for a H266DS Series E2 Heavy Duty Safety Switch?<br /><br />

The parts listed here are the only field replaceable parts.
Complete interior - HN266AE2 (includes line & load base assembly`s, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-214-50 SEL (2-required and arc suppressor assembly is not included)
Load base assembly - 40552-215-50 SEL (2-required)
Arc suppressor assembly - 40512-708-50 SEL (2-required) Obsolete and replaced by 40512-708-50 (2-required)
Lug assembly - 40256-024-50 (2 required per base assembly)
Line base phase insulator - 40512-014-01 (1 required)
Load base phase insulator - 4052-191-01 (1-required)
Line & load base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-191-50 SEL
Vault handle - 40512-194-50 SEL
Handle knob kit (black & red knob at end of handle) - 44011-427-50

CTA-ID : 2054882
Was this helpful?
What can we do to improve the information ?