Technical FAQs

Ask a Question

Is the HCP-SU single row I-Line interior available with unit mounting space less than 54`` so that it could fit into a shorter box?

The HCP-SU single row I-Line interior is only available with 54`` of unit mounting space.


CTA-ID : 2054996
Was this helpful?
What can we do to improve the information ?