Technical FAQs

Ask a Question

Are there electrical accessories for the GFP devices? Does the OFS Auxiliary Switch Adapter, cat.# 26923 work?

Issue:
Are there electrical accessories for the GFP devices? Does the OFS Auxiliary Switch Adapter, cat.# 26923 work?

Product Line:
UL 1053 Listed GFP Ground Fault Protectors

Environment:
Electrical Accessories

Cause:
Some literature says the OFS will work.

Resolution:

On the 4p options, the shunt trip and/or aux switches can be used through the use of the 26923 adapter.

On the 2p, however, there are no electrical accessories as the adapter does not fit the 2p GFP. The OFS does fit the ID Residual Current Switch (IEC rated only), and therefore it would accept electrical accessories.


CTA-ID : 2055512
Was this helpful?
What can we do to improve the information ?